LPC-Link2 Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 Support

10,238件の閲覧回数
lpcware-support
Senior Contributor I

Supported Parts

LPC-Link2 (combined with the associated CMSIS-DAP firmware) is the recommended debug probe for use with LPCXpresso IDE, except for the following MCU families:

  • LPC2xxx (ARM7) , LPC3xxx (ARM9)

    • No support for these parts is planned

For more information on debug probes support by LPCXpresso IDE, please see the FAQ "Which debug probes are supported by LPCXpresso IDE with which MCUs?"

Connection Mechanisms

The "native" way to connect to an LPC-Link 2 is selected by ensuring that link JP1 is not fitted at power on. When used in this manner with LPCXpresso IDE then the latest compatible debug firmware will automatically be downloaded into the probe the first time a debug session is started. This is the recommended way of using an LPC-Link2 with LPCXpresso IDE

It is also possible to use an LPC-Link2 which has been programmed with debug firmware image in flash - by fitting link JP1 before power on.

For more information on programming compatible debug firmware images into LPC-Link2 flash please see LPCScrypt.

LPC-Link2 Board Layout

  146945_146945.pnglpc-link_2_flyer_general.preview.png

ラベル(1)
タグ(2)
0 返答(返信)