lpc802 gpio中断问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc802 gpio中断问题

ソリューションへジャンプ
1,511件の閲覧回数
vector123456
Contributor I

各位,请教一下,LPC802  在SDK中有没有 gpio的中断示例代码?

如果没有的话,能否给一个提示? 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,417件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vector guo,

Yes, as Jeff Chang said, you can find "gpio_led_output" demo under SDK package,

This example shows how to use GPIO with interrupts and make the led shine.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,418件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vector guo,

Yes, as Jeff Chang said, you can find "gpio_led_output" demo under SDK package,

This example shows how to use GPIO with interrupts and make the led shine.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,417件の閲覧回数
vector123456
Contributor I

谢谢!

0 件の賞賛
返信
1,417件の閲覧回数
JeffChang
Contributor III

Yes.  You can find it on the SDK.

SDK--> driver sample code.

0 件の賞賛
返信
1,417件の閲覧回数
vector123456
Contributor I

谢谢!

0 件の賞賛
返信