lpc54618:- Target marked as not debuggable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc54618:- Target marked as not debuggable

1,407 次查看
subodhmankar
Contributor II

Hi,

I have attached 25MHz external clock to custom board.

When I tried to give clock to pll, fro and main using external clock, board doesn't work anymore for me.

I have attached image to this post which is snapshot from Mcuxpresso IDE while I try to debug.

Following is the code generated by MCUxpresso config tool software

/*******************************************************************************

********************** Configuration BOARD_BootClockRUN ***********************

******************************************************************************/

/* clang-format off */

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************

!!Configuration

name: BOARD_BootClockRUN

called_from_default_init: true

outputs:

- {id: CLKOUT_clock.outFreq, value: 25 MHz}

- {id: FRO12M_clock.outFreq, value: 12 MHz}

- {id: FROHF_clock.outFreq, value: 48 MHz}

- {id: FXCOM0_clock.outFreq, value: 12 MHz}

- {id: FXCOM1_clock.outFreq, value: 12 MHz}

- {id: FXCOM2_clock.outFreq, value: 12 MHz}

- {id: FXCOM3_clock.outFreq, value: 12 MHz}

- {id: FXCOM4_clock.outFreq, value: 12 MHz}

- {id: FXCOM5_clock.outFreq, value: 12 MHz}

- {id: FXCOM6_clock.outFreq, value: 12 MHz}

- {id: FXCOMs_CLK32K_clock.outFreq, value: 32.768 kHz}

- {id: MAIN_clock.outFreq, value: 12 MHz}

- {id: SCT_clock.outFreq, value: 12 MHz}

- {id: SPIFI_clock.outFreq, value: 12 MHz}

- {id: SYSPLL_clock.outFreq, value: 25 MHz}

- {id: System_clock.outFreq, value: 12 MHz, locked: true, accuracy: '0.001'}

settings:

- {id: SYSCON.AUDPLLCLKSEL.sel, value: SYSCON._clk_in}

- {id: SYSCON.CLKOUTSELA.sel, value: SYSCON._clk_in}

- {id: SYSCON.FXCLKSEL0.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL1.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL2.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL3.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL4.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL5.sel, value: SYSCON.fro_12m}

- {id: SYSCON.FXCLKSEL6.sel, value: SYSCON.fro_12m}

- {id: SYSCON.M_MULT.scale, value: '16'}

- {id: SYSCON.N_DIV.scale, value: '1'}

- {id: SYSCON.PDEC.scale, value: '16', locked: true}

- {id: SYSCON.SCTCLKSEL.sel, value: SYSCON.MAINCLKSELB}

- {id: SYSCON.SPIFICLKSEL.sel, value: SYSCON.MAINCLKSELB}

- {id: SYSCON.SYSPLLCLKSEL.sel, value: SYSCON._clk_in}

- {id: SYSCON_PDRUNCFG0_PDEN_SYS_PLL_CFG, value: Power_up}

- {id: SYSCON_PDRUNCFG0_PDEN_WDT_OSC_CFG, value: Power_up}

- {id: SYSOSCCTRL_FREQRANGE, value: High}

sources:

- {id: RTC.rtc_32k_osc.outFreq, value: 32.768 kHz, enabled: true}

- {id: SYSCON.WDT_FREQ.outFreq, value: 1 MHz}

- {id: SYSCON._clk_in.outFreq, value: 25 MHz, enabled: true}

* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/

/* clang-format on */

/*******************************************************************************

* Variables for BOARD_BootClockRUN configuration

******************************************************************************/

/*******************************************************************************

* Code for BOARD_BootClockRUN configuration

******************************************************************************/

void BOARD_BootClockRUN(void)

{

/*!< Set up the clock sources */

/*!< Set up FRO */

POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on */

CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch to FRO 12MHz first to ensure we can change voltage without accidentally

being below the voltage for current speed */

POWER_DisablePD(kPDRUNCFG_PD_SYS_OSC); /*!< Enable System Oscillator Power */

SYSCON->SYSOSCCTRL = ((SYSCON->SYSOSCCTRL & ~SYSCON_SYSOSCCTRL_FREQRANGE_MASK) | SYSCON_SYSOSCCTRL_FREQRANGE(1U)); /*!< Set system oscillator range */

POWER_SetVoltageForFreq(25000000U); /*!< Set voltage for the one of the fastest clock outputs: CLKOUT clock output */

CLOCK_SetFLASHAccessCyclesForFreq(12000000U); /*!< Set FLASH wait states for core */

/*!< Set up RTC OSC */

CLOCK_EnableClock(kCLOCK_Rtc); /*!< Enable the RTC peripheral clock */

RTC->CTRL &= ~RTC_CTRL_SWRESET_MASK; /*!< Make sure the reset bit is cleared */

RTC->CTRL &= ~RTC_CTRL_RTC_OSC_PD_MASK; /*!< Setup RTC oscillator */

SYSCON->RTCOSCCTRL = SYSCON_RTCOSCCTRL_EN_MASK; /*!< Setup RTC oscillator clock source availability to other modules */

/*!< Set up WDT OSC */

POWER_EnablePD(kPDRUNCFG_PD_WDT_OSC); /*!< Ensure WDT OSC is off for setup changes */

SYSCON->WDTOSCCTRL = (SYSCON_WDTOSCCTRL_DIVSEL(0) | SYSCON_WDTOSCCTRL_FREQSEL(5)); /*!< Setup WDT oscillator */

POWER_DisablePD(kPDRUNCFG_PD_WDT_OSC); /*!< Ensure WDT OSC is on */

/*!< Set up SYS PLL */

const pll_setup_t pllSetup = {

.pllctrl = SYSCON_SYSPLLCTRL_SELI(20U) | SYSCON_SYSPLLCTRL_SELP(9U) | SYSCON_SYSPLLCTRL_SELR(0U),

.pllmdec = (SYSCON_SYSPLLMDEC_MDEC(63U)),

.pllndec = (SYSCON_SYSPLLNDEC_NDEC(770U)),

.pllpdec = (SYSCON_SYSPLLPDEC_PDEC(11U)),

.pllRate = 25000000U,

.flags = PLL_SETUPFLAG_WAITLOCK | PLL_SETUPFLAG_POWERUP

};

CLOCK_AttachClk(kEXT_CLK_to_SYS_PLL); /*!< Set sys pll clock source*/

CLOCK_SetPLLFreq(&pllSetup); /*!< Configure PLL to the desired value */

/*!< Set up dividers */

CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1U, false); /*!< Reset divider counter and set divider to value 1 */

CLOCK_SetClkDiv(kCLOCK_DivClkOut, 0U, true); /*!< Reset CLKOUTDIV divider counter and halt it */

CLOCK_SetClkDiv(kCLOCK_DivClkOut, 1U, false); /*!< Set CLKOUTDIV divider to value 1 */

CLOCK_SetClkDiv(kCLOCK_DivSctClk, 0U, true); /*!< Reset SCTCLKDIV divider counter and halt it */

CLOCK_SetClkDiv(kCLOCK_DivSctClk, 1U, false); /*!< Set SCTCLKDIV divider to value 1 */

/*!< Set up clock selectors - Attach clocks to the peripheries */

CLOCK_AttachClk(kFRO12M_to_MAIN_CLK); /*!< Switch MAIN_CLK to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM0); /*!< Switch FLEXCOMM0 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM1); /*!< Switch FLEXCOMM1 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM2); /*!< Switch FLEXCOMM2 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM3); /*!< Switch FLEXCOMM3 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM4); /*!< Switch FLEXCOMM4 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM5); /*!< Switch FLEXCOMM5 to FRO12M */

CLOCK_AttachClk(kFRO12M_to_FLEXCOMM6); /*!< Switch FLEXCOMM6 to FRO12M */

CLOCK_AttachClk(kMCLK_to_SCT_CLK); /*!< Switch SCT_CLK to MAIN_CLK */

CLOCK_AttachClk(kMAIN_CLK_to_SPIFI_CLK); /*!< Switch SPIFI_CLK to MAIN_CLK */

CLOCK_AttachClk(kEXT_CLK_to_CLKOUT); /*!< Switch CLKOUT to EXT_CLK */

/* Set SystemCoreClock variable. */

SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;

}

0 项奖励
回复
2 回复数

1,199 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Subodh Mankar,

   At first, please check your external crystal clock with oscilloscope, is your external crystal can oscillate? You must make sure the hardware have no problem.

   Please check it, then give me reply!

Best Regards,

Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,199 次查看
ianbenton
Senior Contributor I

"Target marked as not debuggable" is one of about half a dozen random messages that it gives you when the SWD connection is not working properly. It could be as simple as forgetting to plug the probe in, or switch power to the board, but it's just generally the lack of a decent clock signal. See my post on "Fun and Games with SWD".

Maybe just perhaps you have programmed the chip into some mode where it isn't debuggable, but that's really not that likely. 

0 项奖励
回复