Content originally posted in LPCWare by engineer1 on Wed Oct 22 02:10:23 MST 2014
hi
i have a landtiger board for lpc1768.
Lcd specification:
(
Resolution: QVGA 262K 240*RGB*320
Size: 3.2"
Controller: IL9320
Touch Panel: 4-wire
Pin Pitch: 37Pins & 1mm
2.7-3.3V operating voltage
Backlight: 5 LEDs Parallel
RSM1843 touch panel controller onboard directly compatible with ADS7843
Standard 2.54mm PCB headers for prototyping
Support a SD card interface
)
Someone have ported library's emwin for this board?
thnks!