installing truetype and PNG options for emWIN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

installing truetype and PNG options for emWIN

747 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Robermeyer on Mon Apr 28 10:43:50 MST 2014
From looking at the various manuals its obvious that PNG and truetype font support are not included in the emWin distribution.
The manual says in both cases to download the package and install it.

So what does that mean in an LPC Open world?
Maybe someone that knows could explain what install it would do.
What directory does it go into.
What paths have to be change to get it to compile in?
标签 (1)
0 项奖励
回复
3 回复数

712 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Robermeyer on Thu May 01 13:24:35 MST 2014
t
0 项奖励
回复

712 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Robermeyer on Tue Apr 29 12:28:02 MST 2014
I think I understand the pain of using the truetype driver.
However I can't get it to compile in to try it.
My use of the fonts is generate them and then use them later.  Got lots of RAM laying around.
It will use a lot of RAM but dragging megabytes of font files of different sizes off the flash drive isn't very fast either.
Trying to find some middle ground.

Do you know how to get it to install with the latest LPCopen?
0 项奖励
回复

712 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Mon Apr 28 16:10:48 MST 2014
Can say but one thing.

True type fonts are rendered on the fly from digital data.
You would have to cache the rendered bit maps of suffer the penalty of re-rendering each glyph.
Such a thing would likely drag your performance to it's knees since it is all done in floating point.
just saying.
0 项奖励
回复