find demo binaries for LPC54114 audio and voice recognition kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

find demo binaries for LPC54114 audio and voice recognition kit

448 Views
xiaowei_zhang
Contributor I

Hi everyone,

 

I just ordered a LPC54114 audio and voice recognition kit. But it seems the pre-loaded software with the kit does not have audio and voice recognition function.

 

From NXP website, I download the application not, it says:

 

 pastedImage_1.png

 pastedImage_3.png

I just could not find the pre-built demo binaries software on the given location.

 

Could anyone here to tell me where I can find this pre-built demo binaries software in NXP website, so I can simply download and run the demo.

 

Thanks in the help!

 

Xiaowei

Labels (1)
0 Kudos
Reply
1 Reply

356 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zhang

A demo running on the LPC54114 audio and voice kit (order code OM13090).

This demo shows a system detecting the wake up phrase “Hello Blue Genie”, followed by five other phrases: “Make it so”, “Blink LED”, “Flash display”, “Sensory logo” and “NXP logo”. The demo delivered as a binary file that can be programmed onto the OM13090 board set using a simple drag and drop process.

See attached


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply