I would like to check if below project works property.
lpcopen_2_20_keil_iar_nxp_lpcxpresso_1549\applications\lpc15xx\examples\usbd_rom\cdc_vcom
I already check above project woks property on Windows 10 PC.
Then I want to check if above project works property on Windows 7 PC.
Then I try to download the Windows 7 USB drivers for LPC1549 at below links.
Unfortunately, I cannot download it from above links.
Please tell us where can I download the Windows 7 USB drivers for LPC1549.
Best regards,
Takashima
This issue was solved by removing INTERFACE_ASSOCIATION from bDeviceProtocol in device descriptor.
-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------