When will IBIS models be available for the LPC4357FET256 or can any alternatives be used

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When will IBIS models be available for the LPC4357FET256 or can any alternatives be used

253 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pricey on Mon Feb 20 03:18:34 MST 2012
Hi - I will be starting PCB layout soon for the LPC4357FET256 and will need IBIS models for simulation
1. When will they be available?
2. Presumably they will be the same as those for the LPC4350 in which case when will they be available?
3. I believe that the LPC4350 is very similar to the LPC1850 (apart from M3 vs M4/M0!) would those IBIS models be useable and if so when will they be available?
4. Would the IBIS models for the LPC178x be at all useable / adaptable for this (note looks like different packages)?
Cheers,
Pricey
标签 (1)
0 项奖励
0 回复数