What's the accuracy of LPC5500 powerquad IIR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the accuracy of LPC5500 powerquad IIR

424件の閲覧回数
shaozhongliangs
NXP Employee
NXP Employee

Customer:www.dB-mark.com

Device:LPC5500

 Our customer(www.dB-mark.com) is evaluating LPC5500 PowerQuad computing features. Customer can't find any detial description about "ret" and "ref" in below  formula. Any comment for these two parameters?

1.png 

ラベル(1)
0 件の賞賛
1 返信

352件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello S.z. Liang,

I just got reply from PowerQuad expert of SE team as below:

"

"res" is usually short for "result", which is the result computed by the formula.

"ref" is usually short for "reference", which is the actually result sampled in real condition.

This accuracy computing formula is just to convert the percentage error to dB way. This is no special method here.

"

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛