Hi,
I changed the LPC1769 FBD100 on my 3D printer main board because analog inputs were damaged.
The original was a Rev A and the new one is a Rev C
I have a file "Firmware.bin" that usually burn at starting through the SD card. But not with the new LPC1769...
What checks and actions do you recommend? I'm note very familiar with microcontrolers and I don't have the board shematic.
I also tried to load the firmware with a FTDI usb→serial adapter through UART port and the "Flash Magic" software. It also failed. As described in the datasheet I took care to ground P2.10 pin while pressing the reset button.
Thank you in advance
已解决! 转到解答。
The flash is finally done! Thank you for your help
1) Install a bootloader on the chip is necessary before flashing firmware.bin:
Smoothieware bootloader Download the .hex file
How to flash : You need the FlashMagic software and a PC connected to the board with a FTDI interface.
Press and hold Reset button on the board
Ground input P2.10 on the LPC chip (hold)
Release reset button
Release GND from P2.10
Flash .hex from the software. When transfert is done:
Connect P2.10 to 3.3V for 1s. Wait 10s. Press reset
→ Boot loader is flashed
2) Flash firmware.bin from the SDcard
SDcard maxi 2 Go formated in FAT32 4096 byte
My 3D printer is back to life!
The flash is finally done! Thank you for your help
1) Install a bootloader on the chip is necessary before flashing firmware.bin:
Smoothieware bootloader Download the .hex file
How to flash : You need the FlashMagic software and a PC connected to the board with a FTDI interface.
Press and hold Reset button on the board
Ground input P2.10 on the LPC chip (hold)
Release reset button
Release GND from P2.10
Flash .hex from the software. When transfert is done:
Connect P2.10 to 3.3V for 1s. Wait 10s. Press reset
→ Boot loader is flashed
2) Flash firmware.bin from the SDcard
SDcard maxi 2 Go formated in FAT32 4096 byte
My 3D printer is back to life!
> I have a file "Firmware.bin" that usually burn at starting through the SD card. But not with the new LPC1769...
That sounds very much like the firmware update is to be executed by a proprietary second-stage bootloader.
Which makes me assume your firmware will not run without that BL, even if you manage to flash it onto the MCU. Both are usually integral part of one application, with the BL occupying the reset vector location, doing certain pre-initialisations, and starting the main application at a different adress - usually a different Flash sector.
Hi, Thank you for your help. I'm still not able to flash the LPC1769!
- Uart0 → Checked
- P2.10 start low, and in the end, high → In normal state this pin is high on my board. I grounded the pin when I pressed the reset button and hoped the ISP mode is ON. Is there a way to control?
- USB can be detected by PC with a virtual port → On the FTDI there is some LED that are blinking during transfert so I think the communication PC ↔ FTDI is ok
But what about the baudrate I need to set?
Hi,
Q1)P2.10 start low, and in the end, high → In normal state this pin is high on my board. I grounded the pin when I pressed the reset button and hoped the ISP mode is ON. Is there a way to control?
>>>>It is okay to ground the pin P2.10 pin when you press the reset button
- USB can be detected by PC with a virtual port → On the FTDI there is some LED that are blinking during transfert so I think the communication PC ↔ FTDI is ok
But what about the baudrate I need to set?
>>>The baud rate of uart is 115200. Anyway, pls check if you connect the uart0 pin to the FTDI.
BR
XiangJun Rong
Hi,
First of all, as you know that you have to use uart0 to download code in ISP mode, the P0.2 is TXD0 pin of uart0, the P0.3 is RXD pin of uart0, pls check if the P0.2/P0.3 pins are connected to the FTDI.
Secondly, pls have uart0 to output character and check if the PC serial tools can receive it or not.
BR
XiangJun Rong
Hi,
If you want to download application code to on-chip flash of LPC1769, it is okay to use Flashmagic tools to download *.bin in ISP mode.
1)after Reset, the P2.10 pin must be low so that the LPC can enter ISP mode, after you have downloaded the application code, then you have to configure the P2.10 high so that the application code can be executed.
2)you have to use uart0 pin, in detail, P0.2 is TXD0 pin of uart0, the P0.3 is RXD pin of uart0, the two pins must be connected to the FTDI usb2uart converter.
Pls check if you have connected to uart0 to the FTDI and if the USB can be detected by PC with a virtual port.
Hope it can help you
BR
XiangJun Rong