I want to use the internal oscillator,but the internal oscillator of the LPC1114 does not start。The phenomenon appears as when we use the extern oscillator,the timer can work well ,but when we use the internal oscillator,the same timer can not work.the configurations of the internal oscillator are as follows:
uint32_t i;
 LPC_SYSCON->PDRUNCFG &= ~(1 << 0 | 1 << 1 | 1 << 2 | 1 << 3 | 1 << 5 | 1 << 7); /* Power-up System Osc */
 LPC_SYSCON->SYSOSCCTRL = 0x00000000;晶振不被旁路
 for (i = 0; i < 200; i++) __NOP();
 LPC_SYSCON->SYSPLLCLKSEL = 0x00000001; /* 选择系统时钟 */
 LPC_SYSCON->SYSPLLCLKUEN = 0x01; /* Update Clock Source */
 LPC_SYSCON->SYSPLLCLKUEN = 0x00; /* Toggle Update Register */
 LPC_SYSCON->SYSPLLCLKUEN = 0x01;
 while (!(LPC_SYSCON->SYSPLLCLKUEN & 0x01)); /* Wait Until Updated */
LPC_SYSCON->SYSPLLCTRL = 0x00000003; //系统时钟倍频
 LPC_SYSCON->PDRUNCFG &= ~(1 << 7); /* Power-up SYSPLL */
 while (!(LPC_SYSCON->SYSPLLSTAT & 0x01)); //确定PLL锁定以后向下执行
LPC_SYSCON->MAINCLKSEL = 0x00000000; /* Select 内部振荡器输出 */
 LPC_SYSCON->MAINCLKUEN = 0x01; /* Update MCLK Clock Source */
 LPC_SYSCON->MAINCLKUEN = 0x00; /* Toggle Update Register */
 LPC_SYSCON->MAINCLKUEN = 0x01;
 
					
				
		
 kerryzhou
		
			kerryzhou
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi liu feng,
Please use the CLKOUT pin to test the IRC oscillator and system oscillator at first.
This is the clock block diagram:
If you want to use the IRC oscillator, and use the PLL, in the MAINCLKSEL, you need to select sys_pllclkout, in SYSPLLCLKSEL, you need to select IRC oscillator, not the system oscillator. After the configuration, I suggest you use the CLKOUT pin to test the main clock at first, just make sure your timer have the clock.
Wish it helps you!
If you still have question, please kindly let me know!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
i have solved the problem,thanks