RTOS Supported in MKE14F512VLL16R and LPC54605J256BD100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTOS Supported in MKE14F512VLL16R and LPC54605J256BD100

319 次查看
prasannanaik
Contributor III

Hi,

  Can i know the rtos supported by MKE14F512VLL16R and LPC54605J256BD100. I am looking for a common RTOS for both the microcontrollers.

Thanks and best regards,

Prasanna

标签 (1)
0 项奖励
1 回复

276 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Prasanna Naik ,

Both of these two can be supported by MCUXpresso SDK. But the SDK packages are separated for each device

https://mcuxpresso.nxp.com/en/select 

There is no "one" SDK package supporting these two devices.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励