Hello,
I am trying to use PIO1_5 and PIO1_6 for PWM. PWM works on the PIO1_5 without problems, but not on the PIO1_6. When I set PIO1_6 as CT16B1_MAT1, there is always a log.0, even if EM1 bit changes in the EMR register. This situation executing code with MY_SWITCH = 1.
I have tried to use PIO1_6 as a GPIO pin in order to check if this pin is ok (toggling). It is definitely working properly. Also I changed PIO1_6 to PIO0_16 with CT16B1_MAT1 mode and it works perfectly. This situation executing code with MY_SWITCH = 2.
I tested on two HW - the original LPCXpresso1200 with LPC1227 in LQFP64 case and one on my boards with LPC1227 in LQFP48. Same behaviour on both chips.
Here is the code:
/*
===============================================================================
Name : Test_PWM.c
Author : R-Michalek
Version :
Copyright : $(copyright)
Description : Simple test of PWM on PIO1_5 and PIO1_6
===============================================================================
*/
//#ifdef __USE_CMSIS
#include "LPC122x.h"
//#endif
#include <cr_section_macros.h>
/*
* MY_SWITCH
* = 1 ~ PWM on PIO1_5 and PIO1_6 - wanted version
* = 2 ~ PWM on PIO1_6 and PIO0_16; PIO1_6 is on GPIO mode and toggles in main loop
*/
#define MY_SWITCH 1
#define IOCON_FUNC_0 (0)
#define IOCON_FUNC_1 (1)
#define IOCON_FUNC_2 (2)
#define IOCON_FUNC_3 (3)
#define IOCON_FUNC_4 (4)
#define IOCON_MODE_PULL_UP (1 << 4)
#define IOCON_ADMODE_DIGITAL (1 << 7)
int main(void)
{
volatile unsigned char i = 0;
LPC_SYSCON->SYSAHBCLKCTRL = 0x0001001FUL; // Enable SYS, ROM, RAM, FLASHREG, FLASHARRAY and IOCON
LPC_SYSCON->SYSAHBCLKCTRL |= (0x01 << 8); // Enable CT16B1
LPC_SYSCON->SYSAHBCLKCTRL |= (0x01 << 30); // Enable GPIO1
LPC_SYSCON->SYSAHBCLKCTRL |= (0x01 << 31); // Enable GPIO0
#if MY_SWITCH == 1
LPC_IOCON->PIO1_5 = IOCON_FUNC_3 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT0
LPC_IOCON->PIO1_6 = IOCON_FUNC_3 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
#endif
#if MY_SWITCH == 2
LPC_IOCON->PIO1_5 = IOCON_FUNC_3 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT0
LPC_IOCON->PIO0_16 = IOCON_FUNC_4 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
LPC_IOCON->PIO1_6 = IOCON_FUNC_0 + IOCON_ADMODE_DIGITAL; // GPIO
LPC_GPIO1->DIR |= (1 << 6); // GPIO Output
#endif
// configure CT16B1
LPC_CT16B1->TCR = 0x02; // reset on
LPC_CT16B1->TCR = 0x00; // reset off
LPC_CT16B1->CTCR = 0x00; // Timer mode
LPC_CT16B1->PR = 0x0000; // no pre-scale
LPC_CT16B1->MR0 = 250; // PWM on MAT0 (ratio 1:1)
LPC_CT16B1->MR1 = 250; // PWM on MAT1 (ratio 1:1)
LPC_CT16B1->MR2 = 500; // cycle length
LPC_CT16B1->MCR = (0x01 << 7); // reset on MR2 => cycle length
LPC_CT16B1->CCR = 0x00; // disable all captures
LPC_CT16B1->PWMC = 0x03; // MAT0 and MAT1 is enabled for PWM mode
LPC_CT16B1->EMR = (0x02 << 4) | (0x02 << 6); // set bit EM0 and EM1 to high on match
LPC_CT16B1->TCR = 0x01; // counter enable
// end of configuration
while (1)
{
i = 1 - i;
#if MY_SWITCH == 2
// SetGPIO1(PIO1_6, i);
i ? (LPC_GPIO1->SET = 1<<6) : (LPC_GPIO1->CLR = 1<<6);
#endif
// "Dummy" NOP to allow source level single
// stepping of tight while() loop
__asm volatile ("nop");
}
return 0 ;
}
已解决! 转到解答。
Hi, Rastilav,
Pls refer to the pin assignment, for the P1_6 pin, it appears that you should set the FUNC as 2, but you set it as 3.
Pls use the line
LPC_IOCON->PIO1_6 = IOCON_FUNC_2 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
The following is your original code:
LPC_IOCON->PIO1_6 = IOCON_FUNC_3 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
Hope it can help you
BR
XiangJun Rong
Hi, Rastilav,
Pls refer to the pin assignment, for the P1_6 pin, it appears that you should set the FUNC as 2, but you set it as 3.
Pls use the line
LPC_IOCON->PIO1_6 = IOCON_FUNC_2 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
The following is your original code:
LPC_IOCON->PIO1_6 = IOCON_FUNC_3 + IOCON_ADMODE_DIGITAL; // CT16B1_MAT1
Hope it can help you
BR
XiangJun Rong