OM13092/Keyboard2mouse : how can I run the core at 180Mhz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM13092/Keyboard2mouse : how can I run the core at 180Mhz?

470 次查看
belmontbob59
Contributor IV

 SDK 2.4.1/ Keyboard2mouse  runs the core at 96Mhz. I tried to switch to 180Mhz by replacing the call  BOARD_BootClockFROHF96M() with BOARD_BootClockPLL180M() but it locks up. Is it possible to run the core at 180Mhz with both USB0 (as host ctrl) and USB1 (as device ctrl) active? Why do I need to change in order to achieve this?

thank you

标签 (1)
0 项奖励
1 回复

376 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi bob belmont,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd highly recommend you to use the MCUXpresso Config Tool to build the clock, the tool provides a graphical navigator for the user to configure the clock.
You can learn more information about this tool via the following link:
https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-t...


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励