Content originally posted in LPCWare by wanders on Fri Jan 02 10:27:43 MST 2015
Y'know, I'm in pretty much the same position as the Original Poster. I'm starting with a LPCXpresso board based on the LPC11u14 (which, by the way, is really a fantastic hardware development platform even if it is "obsolete"). I've done all the things in the second post. Really.
What is missing for me is any kind of documentation on LPCOpen 2.0 code. Where is the documentation for the USB libraries (whether flash or ROM)? Do I really have to read example code with no documentation to figure out how the USB library works? Now, THAT'S an unprofessional situation in which I find myself, if true.
So, if it does indeed exist, WTF is the documentation for the LPCOpen 2.0 library?
Thanks in advance,
Wanders