Hi all,
I just created a LPC54102 dual core project in MCUpresso following the guide. (Core M4 = Master, Core M0 = Slave).
After that I want to confiugre the LPC peripherals by MCUXpresso Config Tools but it works only on Master M4 core. When I try to open MCUXpresso Config Tools relative to the Slave core an error message appears :
"The project does not contains any configuration/source file to import open configuration. Open configuration failed due to unknown reason".
What about this issue? I noted that no .mex file appears on Slave project.
What is the correct way to configure the Slave peripherals by MCUXpresso Config Tools?
Thanks.
已解决! 转到解答。
I saw the same issue. Unfortunately I don't have a great solution. I ended up working with a combination of two solutions:
1) Configure the peripheral under the M4 project and then manually copy the configuration code over to the M0+ project.
2) Abandon the MCUXpresso Config Tool for peripherals. It works well for pin assignments and configuring the clocks, but beyond that I found it to be very limiting. I had better results writing the config myself after reading the API Manual and the LPC5410x User manual (UM10850).