LPCXpresso54608 emWin is equipped with 4.3" LCD. If the LCD is changed to 8"~10" LCD,
then the emWin library can still support such a LCD without version updated/?
Hi Gary,
emWin is Segger product, and it is supported by Segger. Please contact Segger for it.
emWin - The Embedded GUI by SEGGER | It simply works!
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------