LPCScrypt dfu-util.exe for LPC1830

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCScrypt dfu-util.exe for LPC1830

Jump to solution
4,275 Views
kensu
Contributor V

Hi

I am using LPC1830,

For LPCScrypt dfu-util.exe,

There is a command -D which can download file to device.

I think the file is download to SRAM.

I want to know where the address the file is download to?

0x10000000?

 

Regards

Ken

 

 

0 Kudos
Reply
1 Solution
4,267 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Could you please point the page you mentioned ?

As I know , LPCscrypt program internal flash and SPIFI flash.

 

BR,

Alice

View solution in original post

0 Kudos
Reply
3 Replies
4,268 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Could you please point the page you mentioned ?

As I know , LPCscrypt program internal flash and SPIFI flash.

 

BR,

Alice

0 Kudos
Reply
4,264 Views
kensu
Contributor V

Hi 

For example:

"LPCScrypt_240.bin.hdr" will be load into device by dfu-util.exe so that lpcscrypt.exe can send command to MCU.

I want to know where the LPCScrypt_240.bin.hdr is load to? 

In my understanding, it should load to SRAM, 0x10000000?

 

Another question is can I get the source code which can build the LPCScrypt_240.bin.hdr?

 

Regards

Ken

0 Kudos
Reply
4,256 Views
kensu
Contributor V

Hi

I got information that I want to know.

I want to creating an image to run from RAM by lpcscrypt.

I get answer from LPCScrypt User Guide page 16.

I will keep to study it.

 

Regards

Ken

 

0 Kudos
Reply