LPC546xx with 1.8V design and USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC546xx with 1.8V design and USB

549 次查看
RU
Contributor I

I want to start a LPC546xx design with 1.8V - how can i use USB0?

标记 (1)
0 项奖励
3 回复数

539 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, pls download the data sheet of LPC546xx from the link:

https://www.nxp.com.cn/docs/en/data-sheet/LPC546XX.pdf

As the following screenshot from above data sheet, you can see that

typical voltage of USB1_AVDD3V3,USB1_AVDDTX3V3 pins are 3.3V

The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:

For USB full-speed operation only 3.0 - 3.6 V
For USB high-speed operation only 1.71 - 3.6 V

the VDDA is from 1.71 to 3.6V.

 

 

xiangjun_rong_0-1657851775481.png

Hope it can help you

BR

XiangJun Rong

 

0 项奖励

499 次查看
RU
Contributor I

Table 12 says for VDD 1.71V .. 3.6V for USB high speed only. According to this, USB would work with 1.8V.

On the other hand, table 21 shows quite contradictory values. Is USB now possible with 1.8V?

RU_0-1659700050452.png

 

0 项奖励

477 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think it is correct:

The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:

For USB full-speed operation only 3.0 - 3.6 V
For USB high-speed operation only 1.71 - 3.6 V

 

Hope it can help you

BR

XiangJun Rong

0 项奖励