Hello,
I am working with LPC54113J256UK49Z and I am unable to get the ROM ISP to respond to the I2C bus. Using the debugger and a sample app I am able to see the probe message on the correct i2c port.
143 >----uint8_t command[] = { SH_CMD_PROBE, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0xA4 };
I am holding both ISP1 (PIO0_4) and ISP0 (PIO0_31) low and toggling the reset pin. I can see that my application is not running. I am issuing the i2c command in a loop, but the pin PIO0_4 remains high.
I do have something connected to the SPI port ( PIO0_12 ) with a 10MEG pull up. I don't know if that is causing an issue or not.
解決済! 解決策の投稿を見る。
I figured out the issues.
-Andy
Hello @Alice_Yang,
I have those signals connected. I am using an iMX6 to program a LPC54113. I am working on completing an in system programming application were the I2C bus on the iMX6 reprograms the LPC54113. I am know the I2C lines are working because when I program my application via SWD I have no issues talking between the host processor and the LPC54113. I also send the ISP probe message to that program and was able to receive it without issue.
The issue I am having is I hold ISP0 and ISP1 low to enter into the boot ROM for I2C/SPI communication I am unable to get ISP to go to 0. My concern is that I have something connected to PIO0_12 which causes the system to think a SPI operation is underway and causes an issue.
I posted the array of the message I was sending in case I was simply reading the reference manual wrong and had a packet format error.
Thanks,
Andy
Hello,
" My concern is that I have something connected to PIO0_12 which causes the system to think a SPI operation is underway and causes an issue."
-> Yes, maybe , how about disconnect PIO0_12.
Also use a logic measure the i2c signal, check whether send right command to LPC54113.
BR
Alice
I figured out the issues.
-Andy
Hello ,
Make sure connect the right I2C signals:
Also could you please describe your application architecture more detail, and the steps to reproduce the issue.
BR
Alice