LPC2468 ADC issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2468 ADC issue

882 次查看
ancymuhammed
Contributor III

We are using the LPC controller LPC2468FET208 ]. We had assembled 72 boards. Out of this 72 boards in 22 boards the ADC readings at higher voltage (above 1.6V) seems to be less than the expected value. We had checked with ADC channel 0, 1 & 6. External reference of 3.3V is given at the VREF pin. In remaining 50 boards all readings are correct. In one of the failed boards after replacing the microcontroller with new one it is working fine. What may be the possible reasons for this

0 项奖励
回复
6 回复数

869 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the data sheet of LPC2468, the Integral non-Linearity spec is +/-2LSB at most.

As you said that just 22 boards out of 72 boards had issue, it appears that this is chip issue.

Anyway, pls check the input source impedance which is connected to ADC analog channel, if it is large, I suggest you develop a buffer based on AMP to convert the impedance.

Hope it can help you

BR

XiangJun Rong

 

 

 

xiangjun_rong_0-1646025462444.png

 

0 项奖励
回复

864 次查看
ancymuhammed
Contributor III

We are giving the output of the pressure sensor to ADC channel . The output of the sensor is given to a voltage divider of value 10K & 20K where 20K is connected to ground and 10K is the series resistor before feeding to the ADC. Also a filtering capacitor of value 10Nf is added at the input of the ADC pin of the controller. We had tried by giving a voltage from the power supply to the ADC directly by removing 10K,20K & 10nf capacitor. But the failure is same. No dip observed in the ADC input of the controller. The input to the controller is correct.

 

 

0 项奖励
回复

855 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you reduce the resistor and the filtering capacitor.

for example using 100 ohm/200 ohm as dividing resistor if possible, using 2.2nF capacitor.

Pls have a try

BTW, if you connect 3.3V to the analog channel of ADC directly, what is the result?

BR

XiangJun Rong

 

0 项奖励
回复

850 次查看
ancymuhammed
Contributor III

While connecting the supply 3.3V, the reading shown is around 875.

 

0 项奖励
回复

819 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It is obvious that the ADC result is 0x3FF or 1023 in decimal if you test 3.3V voltage, but you get 875 in decimal, it is wrong.

Because only part of the boards has the issue, is it possible to contact local FAE so that they can help you.

BR

Xiangjun Rong

0 项奖励
回复

840 次查看
ancymuhammed
Contributor III

We checked the ADC reading by reducing the resistors to 100 & 200. Still we are facing the same issue

0 项奖励
回复