I have been using the LPC213x and 214x for several projects over the years. On each of these projects, I use power down mode in order to save power and to wake up from an external interrupt. On a new project, I wanted a UART1 interrupt and an external event to wake up the processor. Since UART1 is needed, I decided to use Idle Mode. However, I noticed that I am unable to get my external interrupt to wake up on an event. Does Idle Mode not work with External Interrupts? I haven't found specific documentation on that. However, if I go to PD instead, my external interrupt works, so I'm guessing it doesn't work in Idle Mode. If I simulate a external wakeup event and then wake up from a UART1 event, the external interrupt flag is set, but the wakeup from it doesn't occur. Can someone verify if Idle Mode can work with External Interrupts or not, so I can continue investigating or change my design. Thanks in advance.
Also, I don't need an actual interrupt vector. I just need Idle Mode to resume to code. Maybe it can't.
Sutton
解決済! 解決策の投稿を見る。
OK. Here is the answer.
For External Interrupts to wake up the processor from Idle Mode, you MUST have a properly set up ISR associated with EINTx. The ISR is first serviced, then your code will resume execution. Even if your ISR does nothing (except acknowledge the interrupt), it must be there and activated.
On Power-Down, an External Interrupt will resume the code execution without any ISRs, if activated properly.
Hi,
According to the reference manual, Peripheral functions continue operation during Idle mode and may generate interrupts to cause the processor to resume execution.
So it is possible to generate external interrupts in Idle mode.
Regards
Soledad
I think the interrupts the manual is talking about is from internal
interrupts from peripherals and not the external interrupt pin. I have
been unable to ever get a wake up from Idle Mode from an External
Interrupt, but it works 100% in Power Down Mode.
Sutton Mehaffey
Lookout Portable Security
4105 Royal Dr. #100
Kennesaw, GA 30144
770-514-7999
770-514-1285 (FAX)
www.lookoutportablesecurity.com
sutton@lookoutportablesecurity.com
Hi,
EINT0 may be used to wake up the processor from Idle or Power-down modes.
Regards
Soledad
And then, in the External interrupt section, it only says Power-Down Mode.
4.5 External interrupt inputs
The LPC213x includes four External Interrupt Inputs as selectable pin functions. The External Interrupt Inputs can optionally be used to wake up the processor from Power-down mode.
4.5.1 Register description
The external interrupt function has four registers associated with it. The EXTINT register contains the interrupt flags, and the EXTWAKEUP register contains bits that enable individual external interrupts to wake up the microcontroller from Power-down mode.
OK. Here is the answer.
For External Interrupts to wake up the processor from Idle Mode, you MUST have a properly set up ISR associated with EINTx. The ISR is first serviced, then your code will resume execution. Even if your ISR does nothing (except acknowledge the interrupt), it must be there and activated.
On Power-Down, an External Interrupt will resume the code execution without any ISRs, if activated properly.
Thanks. I did read that. But, so far I still have been unsuccessful getting ENT3 to wake up the processor from Idle Mode. ENT3 wakes it up every time on Power Down mode every time.