LPC1788 lpcusblib里面只对port 1做处理 ,没有对port2做处理

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 lpcusblib里面只对port 1做处理 ,没有对port2做处理

1,950 Views
mini92
Contributor I

我在调试lpc1788的usb host部分时候发现 

lpcusblib的ohci.c中只针对 port1 处理没有针对port2 做处理

if (IntStatus & HC_INTERRUPT_RootHubStatusChange) { //´¦Àí root hubµÄ״̬¸ü¸Ä ÓÐ
for(;USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_StatusChangeMask;){
/* only 1 port/host --> skip to get the number of ports */ //ÕâÀïÖ»´¦ÀíÁË USB1µÄÇé¿öûÓд¦Àí USB2µÄÇé¿ö ..À¬»ø¿â
if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_ConnectStatusChange) {
if (USB_REG(HostID)->RhStatus & HC_RH_STATUS_DeviceRemoteWakeupEnable) { /* means a remote wakeup event */ //Ô¶³Ì»½ÐÑ

}
else {}

USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_ConnectStatusChange; /* clear CSC bit */ //¼ì²âµ½²åÈë »òÕ߰γöʼþ
OHciRhStatusChangeIsr(HostID, USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_CurrentConnectStatus);
}

if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortEnableStatusChange) {
USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortEnableStatusChange; /* clear PESC */ //½«¶Ë¿ÚʹÄÜ
}

if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortSuspendStatusChange) {
USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortSuspendStatusChange; /* clear PSSC */ //¹ÒÆð´Ë¶Ë¿Ú
}

if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_OverCurrentIndicatorChange) { /* Over-current handler to avoid physical damage */
USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_OverCurrentIndicatorChange; /* clear OCIC */ //½áÊøʲô ָʾ·û±êÖ¾
}

if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortResetStatusChange) {
USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortResetStatusChange; /* clear PRSC */ //Èí¼þ¸´Î»¶Ë¿Ú
}
}
}

Labels (1)
0 Kudos
6 Replies

1,535 Views
mini92
Contributor I

Hi,

   Thank you ask me , I've changed that before that,  but enum device stop in pipe get device description  in

 host.c

if ((SubErrorCode = USB_Host_SendControlRequest(corenum, &DevDescriptor)) != HOST_SENDCONTROL_Successful) { //sendControlRequest
ErrorCode = HOST_ENUMERROR_ControlError;
break;
}
DEBUGOUT("Get devicedescription\r\n"); //
USB_Host_ControlPipeSize[corenum] = DevDescriptor.Endpoint0Size;

Pipe_ClosePipe(corenum, PIPE_CONTROLPIPE);

debug is stoping this function:

static HCD_STATUS WaitForTransferComplete(uint8_t EdIdx)
{
#ifndef __TEST__ 
while ( HcdED(EdIdx)->status == HCD_STATUS_TRANSFER_QUEUED ) {}
return (HCD_STATUS) HcdED(EdIdx)->status;
#else
return HCD_STATUS_OK;
#endif
}

0 Kudos

1,287 Views
shivrajtbm
Contributor I

hi, 

mini92

have you got any solution for this particular issue..??

i am facing similar issue .. can u plz help!

0 Kudos

1,535 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Chao Li,

Are you also modifying the lpcusblib_MassStorageHost example of lpcopen for lpc1788? Are you testing it on an evaluation board? Please make sure you are implementing the changes described above.

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 Kudos

1,535 Views
ulyssesfonseca
Contributor II

Hi Carlos Mendoza

I'm also with the same problem with Chao Li, my code are stoping in the function 

static HCD_STATUS WaitForTransferComplete(uint8_t EdIdx)

I have made the modifications described above like you.

0 Kudos

1,535 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Chao Li,

This is what I changed on lpcusblib_MassStorageHost example of lpcopen 2.10 for lpc1788 and it can work fine on usb port 2 on EA lpc1788 board.:

 

In HAL_LPC17xx.h I added a MACRO to switch between USB port 1 and port 2

#define USB_PORT_1                    0‍

 

In HAL_LPC17xx.c, I modified IOCON configuration:

#if USB_PORT_1
     Chip_IOCON_PinMux(LPC_IOCON, 0, 29, IOCON_MODE_INACT, IOCON_FUNC1);     /* P0.29 D1+, P0.30 D1- */
     Chip_IOCON_PinMux(LPC_IOCON, 0, 30, IOCON_MODE_INACT, IOCON_FUNC1);
#else
     Chip_IOCON_PinMux(LPC_IOCON, 0, 31, IOCON_MODE_INACT, IOCON_FUNC1);     /* P0.31 D2+ */
     //Chip_IOCON_PinMux(LPC_IOCON, 1, 30, IOCON_MODE_INACT, IOCON_FUNC1); /* P1.30 USB_PWRD2 */
     //Chip_IOCON_PinMux(LPC_IOCON, 1, 31, IOCON_MODE_INACT, IOCON_FUNC1); /* P1.31 USB_OVRCR2 */
#endif

#if defined(USB_CAN_BE_HOST)
#if USB_PORT_1
     Chip_IOCON_PinMux(LPC_IOCON, 1, 19, IOCON_MODE_INACT, IOCON_FUNC2);     /* USB_Power switch */
#else
     Chip_IOCON_PinMux(LPC_IOCON, 0, 12, IOCON_MODE_INACT, IOCON_FUNC1);     /* USB_PPWR2 */
#endif
#endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

 

And finally, on OHCI.c file, I changed. In HcdInitDriver function:

#if USB_PORT_1
     USB_REG(HostID)->StCtrl = 0x1;                         /* Port 1 is host */
#else
     USB_REG(HostID)->StCtrl = 0x00;                     /* Port 2 is host */
#endif‍‍‍‍‍

 

In same OHCI.c file, I replace next functions to substitute RhPortStatus1 by RhPortStatus2:

#if USB_PORT_1
HCD_STATUS HcdGetDeviceSpeed(uint8_t HostID, HCD_USB_SPEED *DeviceSpeed)
{
     if ( USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_CurrentConnectStatus) {     /* If device is connected */
          *DeviceSpeed =
                    ( USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_LowSpeedDeviceAttached) ? LOW_SPEED : FULL_SPEED;
          return HCD_STATUS_OK;
     }
     else {
          return HCD_STATUS_DEVICE_DISCONNECTED;
     }
}

uint32_t HcdGetFrameNumber(uint8_t HostID)
{
     return ohci_data[HostID].hcca.HccaFrameNumber;
}

HCD_STATUS HcdRhPortReset(uint8_t HostID)
{
     HcdDelayMS(400);// TODO delay should be on Host_LPC
     USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortResetStatus;     /* SetPortReset */
     /* should have time-out */
     while ( USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortResetStatus) {}

     USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortResetStatusChange;/* Clear Port Reset Status Change */

     HcdDelayMS(400);// TODO delay should be on Host_LPC
     return HCD_STATUS_OK;
}

HCD_STATUS HcdRhPortEnable(uint8_t HostID)
{
     USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PowerEnableStatus;/* SetPortEnable */

     return HCD_STATUS_OK;
}

HCD_STATUS HcdRhPortDisable(uint8_t HostID)
{
     USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_CurrentConnectStatus;     /* ClearPortEnable */

     return HCD_STATUS_OK;
}
#else
HCD_STATUS HcdGetDeviceSpeed(uint8_t HostID, HCD_USB_SPEED *DeviceSpeed)
{
     if ( USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_CurrentConnectStatus) {     /* If device is connected */
          *DeviceSpeed =
                    ( USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_LowSpeedDeviceAttached) ? LOW_SPEED : FULL_SPEED;
          return HCD_STATUS_OK;
     }
     else {
          return HCD_STATUS_DEVICE_DISCONNECTED;
     }
}

uint32_t HcdGetFrameNumber(uint8_t HostID)
{
     return ohci_data[HostID].hcca.HccaFrameNumber;
}

HCD_STATUS HcdRhPortReset(uint8_t HostID)
{
     HcdDelayMS(400);// TODO delay should be on Host_LPC
     USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PortResetStatus;     /* SetPortReset */
     /* should have time-out */
     while ( USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_PortResetStatus) {}

     USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PortResetStatusChange;/* Clear Port Reset Status Change */

     HcdDelayMS(400);// TODO delay should be on Host_LPC
     return HCD_STATUS_OK;
}

HCD_STATUS HcdRhPortEnable(uint8_t HostID)
{
     USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PowerEnableStatus;/* SetPortEnable */

     return HCD_STATUS_OK;
}

HCD_STATUS HcdRhPortDisable(uint8_t HostID)
{
     USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_CurrentConnectStatus;     /* ClearPortEnable */

     return HCD_STATUS_OK;
}
#endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

And finally, in HcdirqHandler function RhPortStatus1 must be changed by RhPortStatus2:

#if USB_PORT_1
     /* Process RootHub Status Change */
     if (IntStatus & HC_INTERRUPT_RootHubStatusChange) {
          for(;USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_StatusChangeMask;){
               /* only 1 port/host --> skip to get the number of ports */
               if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_ConnectStatusChange) {
                    if (USB_REG(HostID)->RhStatus & HC_RH_STATUS_DeviceRemoteWakeupEnable) {     /* means a remote wakeup event */

                    }
                    else {}

                    USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_ConnectStatusChange;     /* clear CSC bit */
                    OHciRhStatusChangeIsr(HostID, USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_CurrentConnectStatus);
               }

               if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortEnableStatusChange) {
                    USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortEnableStatusChange;     /* clear PESC */
               }

               if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortSuspendStatusChange) {
                    USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortSuspendStatusChange;               /* clear PSSC */
               }

               if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_OverCurrentIndicatorChange) {     /* Over-current handler to avoid physical damage */
                    USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_OverCurrentIndicatorChange;               /* clear OCIC */
               }

               if (USB_REG(HostID)->RhPortStatus1 & HC_RH_PORT_STATUS_PortResetStatusChange) {
                    USB_REG(HostID)->RhPortStatus1 = HC_RH_PORT_STATUS_PortResetStatusChange;               /* clear PRSC */
               }
          }
     }
#else
     /* Process RootHub Status Change */
     if (IntStatus & HC_INTERRUPT_RootHubStatusChange) {
          for(;USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_StatusChangeMask;){
               /* only 1 port/host --> skip to get the number of ports */
               if (USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_ConnectStatusChange) {
                    if (USB_REG(HostID)->RhStatus & HC_RH_STATUS_DeviceRemoteWakeupEnable) {     /* means a remote wakeup event */

                    }
                    else {}

                    USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_ConnectStatusChange;     /* clear CSC bit */
                    OHciRhStatusChangeIsr(HostID, USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_CurrentConnectStatus);
               }

               if (USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_PortEnableStatusChange) {
                    USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PortEnableStatusChange;     /* clear PESC */
               }

               if (USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_PortSuspendStatusChange) {
                    USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PortSuspendStatusChange;               /* clear PSSC */
               }

               if (USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_OverCurrentIndicatorChange) {     /* Over-current handler to avoid physical damage */
                    USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_OverCurrentIndicatorChange;               /* clear OCIC */
               }

               if (USB_REG(HostID)->RhPortStatus2 & HC_RH_PORT_STATUS_PortResetStatusChange) {
                    USB_REG(HostID)->RhPortStatus2 = HC_RH_PORT_STATUS_PortResetStatusChange;               /* clear PRSC */
               }
          }
     }
#endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos

1,535 Views
mini92
Contributor I

Hi,

 

   Thank you ask me , I've changed that before that,  but enum device stop in pipe get device description  in

 host.c

 

if ((SubErrorCode = USB_Host_SendControlRequest(corenum, &DevDescriptor)) != HOST_SENDCONTROL_Successful) { //sendControlRequest
ErrorCode = HOST_ENUMERROR_ControlError;
break;
}
DEBUGOUT("Get devicedescription\r\n"); //
USB_Host_ControlPipeSize[corenum] = DevDescriptor.Endpoint0Size;

Pipe_ClosePipe(corenum, PIPE_CONTROLPIPE);

 

 

debug is stoping this function:

static HCD_STATUS WaitForTransferComplete(uint8_t EdIdx)
{
#ifndef __TEST__ 
while ( HcdED(EdIdx)->status == HCD_STATUS_TRANSFER_QUEUED ) {}
return (HCD_STATUS) HcdED(EdIdx)->status;
#else
return HCD_STATUS_OK;
#endif
}

0 Kudos