LPC1754求助

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1754求助

595 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SZ13039 on Thu Dec 06 21:52:21 CST 2012
项目需要至少6个AD和4个串口。目前选型芯片为LPC1754。但1754这个芯片,根据数据手册,两路AD和串口功能复用,无法满足,也就是最多4个AD和4个串口或者6路AD和3个串口。麻烦确认一下该问题,或者有其他型号推荐。
项目必须:PIN脚备注:
AD部分P0.2/TXD0/AD0.779
P0.3/RXD0/AD0.680
P0.25/AD0.2/I2SRX_SDA/TXD37
P0.26/AD0.3/AOUT/RXD36
P1.30/VBUS/AD0.418
P1.31/SCK1/AD0.517
I2C部分P0.27/SDA0/USB_SDA25
P0.28/SCL0/USB_SCL24
串口部分P0.15/TXD1/SCK0/SCK47
P0.16/RXD1/SSEL0/SSEL48
P2.8/TD2/TXD2/ENET_MDC50
P2.9/USB_CONNECT/RXD2/ENET_MDIO49
P4.29/TX_MCLK/MAT2.1/RXD368
P4.28/RX_MCLK/MAT2.0/TXD365


Labels (1)
0 Kudos
Reply
1 Reply

573 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric.wang@nxp.com on Thu Dec 06 22:18:43 CST 2012
谢谢你的问题。我看了一下LPC175x的数据手册。的确存在这个问题,UART0和AD0.6和AD0.7都没有多余的引脚选择。建议你增加一些外围来实现。
0 Kudos
Reply