Hi,
I am running Windows 10 with a fresh install of MCUXpresso IDE v11.2.0 [Build 1420] [2020-07-09]. I can clean and build the example freetos_blinky project, but I am running into issues debugging it. I cannot debug my LPCXpresso (LPC1549) V2 Rev C board. The Debug Probe shows up fine as LPC-LINK2 CMSIS-DAP V5.361 with no driver errors.
My issue seems exactly like that found here,
https://community.nxp.com/message/1097643
however the configuration changes in the solution are not available in my version of the MCUXpresso IDE.
I've struggled to find a solution online. Help would be much appreciated.
Ian, I am using the LPC1549 evaluation board. The LPCXpresso (LPC1549) V2 Rev C board. After having issues, I've purchased a second one to try to rule out a hardware issue. I've also used multiple USB cables that have worked in other projects. I've mentioned jumper locations and USB port above. I'm not sure where else to go for hardware issues.
I am new to the NXP platform, so I'm not sure if I'm missing a step regarding entering ISP mode or something similar.
Hello eric Lockman,
What about your debug issue, please take a video or screenshot show your steps.
Regards,
Alice
Hello Eric,
I just test the gpio demo under LPCopen, debug well.
Could you please delete the .metadata folder under workspace, then restart MCUXpresso IDE,
import a simple new demo, reconnect your board, check whether can work well.
If still can't , how about change another USB cable, reinstall IDE? Or test another new board?
Regards,
Alice
Thank you again, Alice.
I tried deleting the .metadata folder and restarting the IDE. I tried different USB cables. I tried reinstalling the IDE. None of these produced positive results.
Next, I installed FlashMagic (from Flash Magic - Download) to try to read the chip signature. This has failed during baud rate detection.
I a just ordered a new development board and will report the results.
Alice, I've tried all suggestions above, including purchasing a second development board. I have the same results. Do I need to enter ISP mode with the push-buttons, or something similar in order to Flash the board?
alicewang, thank you for your quick response.
This is my first project with an NXP platform, but I've used Eclipse IDE in the past. I downloaded and installed the MCUXpresso IDE and imported the LPC1549 sample projects. I made sure that the freetos_blinky project was selected, then used the Quickstart Panel to clean and build the project. The images below show my MCUXpresso IDE version and the project having been built successfully.
Once the project was built, I again used the Quickstart Panel to Debug. The LinkServer probe was detected.
However, the download fails with the errors shown below.
These screen captures provide Console and Debugger Console outputs:
The similar question referenced in the OP suggested disabling the "enhanced peripheral service," however my version does not provide that option in the LinkServer Options page.
I appreciate the help, please let me know if I can provide more feedback.