Hi,
I have some issues using LPC55S06-EVK for SECURE-BOOT and SBKEK/USERKEK AES Keys.
Secure Boot is enable, SWD is disable and can only be enable using Secure Debug but I have some issue with nxpdebugmbox auth and with internal Key (USERKEK, SBKEK).
PFR region is not sealed.
How can I reconfigure the dev kit as it come from factory ? ( i know tha cfpa version should be increment each time).
For exemple, I want to disable secure boot and remove all key/allocation code.
Thanks for your help.
I hope you are doing well.
You can try to set the MCU to boot plain images again using below settings on the elftosb gui. This is only in the CMPA.
However, for this we need to have ISP enabled.
All the best,
Diego.
Did you continued to have issues obtaining the tool? Or where you able to recover any of your parts?
Diego
I hope you are doing well!
I am afraid that there we do not have a method to restore the chip's PFR ( for example ,restore CMPA and CPFA) as the chip comes from factory.
Generally speaking, if the PFR section is not sealed, you may try to restore several fields but there is a very high risk of bricking your part.
Are you able to show us your errors with Debug mailbox and the procedure you followed ? So we can try to determine the issue.
Let me know if there is any other question you may have.
All the best,
Diego.
I hope you are doing well!
I am afraid that there we do not have a method to restore the chip's PFR ( for example ,restore CMPA and CPFA) as the chip comes from factory.
Generally speaking, if the PFR section is not sealed, you may try to restore several fields but there is a very high risk of bricking your part.
Are you able to show us your errors with Debug mailbox and the procedure you followed ? So we can try to determine the issue.
Let me know if there is any other question you may have.
All the best,
Diego.
Hi,
I try to use MCUXpresso Secure Provisioning to come back in unsigned mode .
All command success (send empty CMPA, erase flash , and send binary) but since I can't connect with blhost, nxpdebugmbox and SWD is still not accessible.
The CMPA /CFAP is those i previously send