Has anyone tried keyword sporting using CMSIS-NN on ARM Cortex M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone tried keyword sporting using CMSIS-NN on ARM Cortex M4

669件の閲覧回数
vishal_roy
Contributor II

Trying to get Realtime KWS working on OM13098.Two issues I have is not sure what would be the best setting for MIC module and secondly the data transfer mechanism from mic DMA to CMSIS-NN feature extraction modules. I was able to get the demo working on this platform. But in this case the audio input was hardcoded data. 

ラベル(6)
0 件の賞賛
1 返信

561件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Vishal,

Hope you are doing well. At the moment this is not supported with the LPC546xx. Did you use the following guide to port the examples to your board?

Best Regards,

Sabina

0 件の賞賛