EMC_Reset_Disable bit - where is it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMC_Reset_Disable bit - where is it?

2,050 Views
kbarker
Contributor I

The user manual UM10503 for the LPC43xx microcontrollers, in the External Memory Controller (EMC) chapter mentions the EMC_Reset_Disable bit, which controls whether or not parts of the EMC are reset during a warm reset.

However, there is no information on where the EMC_Reset_Disable bit is.

What is the address of the register that the EMC_Reset_Disable bit is in?

Which bit is it within that register?

What is the default (POR) value of the EMC_Reset_Disable bit?

Labels (1)
0 Kudos
Reply
2 Replies

1,908 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the EMC status register. 

pastedImage_1.png

I hope this helps, 

have a nice day!

Regards 

Soledad

0 Kudos
Reply

1,908 Views
kbarker
Contributor I

Thank you for your reply, but it does not answer the question.

The EMC status register is read-only and there's no information on which bit (if any) is the EMC_Reset_Disable bit.

In other microcontrollers, there is (apparently) a ...

 "configuration bit in the SCS register, called EMC_Reset_Disable ..."

However, I can't find any information on where this is for the LPC4350.

0 Kudos
Reply