Brown out BOD voltage levels LPC433x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Brown out BOD voltage levels LPC433x

606 Views
radomirkozub-re
NXP Employee
NXP Employee

Hello,

 

can somebody help me where to find voltage levels of BOD, both interrupt and reset.

 

User manual implicates that there are four levels of BOD voltage threshold, Level 0 to Level 3

 

 

 

however in data sheet there is are only two levels Level 2 and Level 3  mentioned.

 

 

Any idea?

 

Many thanks

 

Radomir

Labels (1)
0 Kudos
1 Reply

459 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Radomir,

I beleive those levels were left out of that datasheet because the reset assertion points are quite far from the minimum operating VDD voltage. But you can still use the values from the LPC4350/30/20/10 datasheet as reference:

https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos