Are the PLU volatile or non-volatile? (in LPCxpresso55s69)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the PLU volatile or non-volatile? (in LPCxpresso55s69)

664 Views
randa_zarrouk
Contributor III

The LPC55xx include a PLU (Programmable Logic Unit) which is used to create small combinatorial and/or sequential logic networks including simple state machines.
My question: is the PLU volatile or non-volatile?

Labels (2)
3 Replies

570 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Randa Zarrouk ,

Volatile. 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

570 Views
randa_zarrouk
Contributor III

Hello Alice_Yang‌, thank you for the response.

When is the configuration of the PLU is exactly done? Is it automatically conducted just after the start-up of the device?

Is there any reference that is explaining that in more details? I want to refer to that in one of scientific publications. 

kind regards, 

0 Kudos
Reply

570 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Randa Zarrouk,

There is PLU demo under SDK package for LPC804, the PLU module is the same between LPC55s69 and LPC804.

You can download the SDK from:  https://mcuxpresso.nxp.com/en/select  

Then you can refer to the demo with User Manual .


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------