Note: This document provides a simple description, the details about flashloader can be found at Getting Started with LPC540xx Flashloader User's Guide.pdf which is located in SDK_2.5.0_LPCXpresso54S018\middleware\mcu-boot\doc
| 
 Boot mode  | 
 ISP2 PIO0_6 pin  | 
 ISP1 PIO0_5 pin  | 
 ISP0 PIO0_4 pin  | 
 Description  | 
| 
 USB1 DFU boot  | 
LOW | LOW | HIGH | 
 USB DFU class is used to download image over the USB1 high-speed port into SRAM.  | 
Connect the LPC54S0xx device USB1 high-speed port and PC with USB. The following is the command line to load the flashloader.bin:
$ dfu-util.exe –D flashloader.bin
Once the flashloader binary is downloaded and starts its execution on the LPC54S0xx platform and there remains a physical USB connection between the LPC54S0xx platform USB1(High-Speed) and host, the flashloader will be ready to receive the commands.
Note: xxx.bin is the target file which needs to be downloaded to the flash.
Author: Hao Liu
Thanks for Hao Liu.
Dear Alice-san,
$ dfu-util.exe –D flashloader.bin
I think I need a driver before doing the above, where can I get the driver?
Best Regards,
Yasushi Hasegawa