Ethernet operation when the MAC is operated at a tenth (5MHz) of the expected speed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet operation when the MAC is operated at a tenth (5MHz) of the expected speed.

1,102件の閲覧回数
lpcware-support
Senior Contributor I

Question:
If the RMII interface is provided to the physical transmission medium (PHY) and this provided a reference clock to the MAC (that is integrated into the microcontrollers) and operated at a tenth of the expected speed (i.e. 5MHz), would everything still work (the data communication system is intended to operate as 10Mb/s Ethernet, but at reduced data rate of 1Mb/s)?

Answer:
Running at a slower reference clock should still work, however it is not guaranteed

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)