Ethernet operation when the MAC is operated at a tenth (5MHz) of the expected speed.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet operation when the MAC is operated at a tenth (5MHz) of the expected speed.

1,136 次查看
lpcware-support
Senior Contributor I

Question:
If the RMII interface is provided to the physical transmission medium (PHY) and this provided a reference clock to the MAC (that is integrated into the microcontrollers) and operated at a tenth of the expected speed (i.e. 5MHz), would everything still work (the data communication system is intended to operate as 10Mb/s Ethernet, but at reduced data rate of 1Mb/s)?

Answer:
Running at a slower reference clock should still work, however it is not guaranteed

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数