silex dev. board SX-ULPAN-EVK usage with KDS 3.0 and KSDK 1.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

silex dev. board SX-ULPAN-EVK usage with KDS 3.0 and KSDK 1.2.0

519 Views
ThomNet
Contributor III

Hi,

 

does anyone used the above mentioned board SX-ULPAN-EVK already with KDS 3.0 /KSDK 1.2.0.

 

If yes: Is there a demo project available, i.e. httpsrv or web-hvac?

 

Any comment is highly appreciated! Thanks in advance

 

Thomas

Labels (1)
0 Kudos
1 Reply

388 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Thomas,

no, for the evaluation kit SX-ULPAN-EVK is MQX support but no support of KSDK and KDS, but if I see the SX specifications SX-ULPAN-EVK | Evaluation Kits | Silex Technology America

and you have also TWR-K21F120M, there is support of KSDK 1.2 and KDS 3.0 but not for mentioned demos.

You mentioned demo web_hvac and httpsrv.

Demo for Heating, Ventilating, and Air Conditioning on lwIP TCP/IP Stack and HTTP Server Demo on lwIP TCP/IP Stack are available for FRDM-K64F, TWR-K60D100M, TWR-K64F120M and TWR-K65F180M.

I attach you documentation for KSDK examples.

I hope it helps you,

Best Regards,

Iva

0 Kudos