Will the KV10 or KV11 be supported in Kinetis SDK v2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Will the KV10 or KV11 be supported in Kinetis SDK v2?

跳至解决方案
615 次查看
kylemanna
Contributor II

Will the KV10 or KV11 be supported in Kinetis SDK v2?  I see that they are supported in Kinetis SDK v1.3, but I'd like to use v2.0.

 

Thanks!

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
480 次查看
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

在原帖中查看解决方案

0 项奖励
回复
2 回复数
481 次查看
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

0 项奖励
回复
480 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Kyle,

no, only these details in the document are relevant.

No early access is not possible.

Best Regards,

Iva

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复