Will the KV10 or KV11 be supported in Kinetis SDK v2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will the KV10 or KV11 be supported in Kinetis SDK v2?

Jump to solution
702 Views
kylemanna
Contributor II

Will the KV10 or KV11 be supported in Kinetis SDK v2?  I see that they are supported in Kinetis SDK v1.3, but I'd like to use v2.0.

 

Thanks!

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
567 Views
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

View solution in original post

0 Kudos
Reply
2 Replies
568 Views
kylemanna
Contributor II

Dug deeper, it appears it's slated for July 2016 as documented here: Introducing Kinetis SDK v2

Anyway to get access to an early release?

0 Kudos
Reply
567 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Kyle,

no, only these details in the document are relevant.

No early access is not possible.

Best Regards,

Iva

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply