Regard to the cdc endpoint in usb composite ( cdc + msd )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regard to the cdc endpoint in usb composite ( cdc + msd )

跳至解决方案
2,335 次查看
jimhuang2
Contributor III

Hello,

I create the usb composite cdc msc project, and I'm going  to see usb_device_descriptor.c/.h, I don't understand that Bulk IN and Bulk OUT endpoint number is same in the endpoint descriptor of Data Interface descriptor (below picture : Green wire).

pastedImage_4.bmppastedImage_3.bmp

I try to change Bulk OUT number 3 to number 5, This change will cause cdc to don't work. 

pastedImage_1.bmp

I think it is related to the driver(INF), but not very sure.

Why the Bulk IN and Bulk OUT endpoint number is same?

Best Regards,

Jim

标记 (1)
0 项奖励
回复
1 解答
2,145 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Jim,

Please see the USB 2.0 specification. In section 5.3.1.2, it shows

"Functions can have additional endpoints as required for their implementation. Low-speed functions are
limited to two optional endpoints beyond the two required to implement the Default Control Pipe. Fullspeed
devices can have additional endpoints only limited by the protocol definition (i.e., a maximum of 15
additional input endpoints and 15 additional output endpoints)."

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,144 次查看
jimhuang2
Contributor III

Hi Jing,

I am going to see 5.3.1.2 Non-endpoint Zero Requirements, but the next chapter "5.3.2. Stream Pipes" have describe  

 

Stream pipes deliver data in the data packet portion of bus transactions with no USB-required structure on
the data content. Data flows in at one end of a stream pipe and out the other end in the same order. Stream
pipes are always uni-directional in their communication flow.

 

A stream pipe to a device is bound to a single device endpoint number in the appropriate direction (i.e.,
corresponding to an IN or OUT token as defined by the protocol layer). The device endpoint number for the
opposite direction can be used for some other stream pipe to the device.

 

Stream pipes support bulk, isochronous, and interrupt transfer types, which are explained in later sections.

 

So, I think an endpoints number only set one transmission direction.

 

Best Regards,

Jim

0 项奖励
回复
2,144 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

No. For example, the pipe on endpoint 1 out and endpoint 1 in is different pipe, they are different endpoint.

Regards,

jing

0 项奖励
回复
2,146 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Jim,

Please see the USB 2.0 specification. In section 5.3.1.2, it shows

"Functions can have additional endpoints as required for their implementation. Low-speed functions are
limited to two optional endpoints beyond the two required to implement the Default Control Pipe. Fullspeed
devices can have additional endpoints only limited by the protocol definition (i.e., a maximum of 15
additional input endpoints and 15 additional output endpoints)."

Regards,

Jing

0 项奖励
回复
2,144 次查看
jimhuang2
Contributor III

Thank you for your reply, I tested that IN and OUT endpoint number is same to work. 

0 项奖励
回复