I installed KSDK 1.2.0, KDS 3.0.0, PE 10.4 and JLink V500, installed the KSDK a second time in KDS via help/install (because the
"installation program" is only a self-extracting archive) and then a third time the same way and now it can't be installed a fourth time because it is already installed:
So now it is fully installed.
I also set the environment variable KSDK_PATH, but i still don't have a KSDK when i start a new Kinetis project for a processor (MK60DN256ZVLL10):
This results in strange errors like my code in the loop in main.c gets deleted and when i am using PE, and many components are shown but not availible, e. g. for gpio1:fsl_gpio i get the error "is not installed in this version of ProcessorExpert".
And without PE i can use no component, so i can use nothing; even LED blinking is not possible!
How can i start a new project with KSDK?
解決済! 解決策の投稿を見る。
Hello Rolf,
yes - it is right, because MK60DN256ZVLL10 is actually no supported by current KSDK 1.2.
So what can I recommend you it use to supported devices. These devices you find at Release Note
I hope this helps you,
Iva
Thanks for the answers, but the problem is that i have a board with an MK60DN256ZVLL10 which shold work in a product in a few months.
So what can i do?
Is there a way to use KDS without KSDK?
I tried that but without KSDK i have no components, so nearly nothing.
And what are the alternatives to KDS, for the MK60DN256ZVLL10?
Thanks for the answer, but can the platform library for KDS build the same way as for IAR, as described in the migration guide?
How much work (mandays) is necessary for such a migration?
And does this give me the components, e. g. for the GPIO pins for LED toggling?
Hello Rolf,
Yes, it is the same procedure for KDS.
It can take few days, not whole week.
Yes, it will be the same support like for supported devices.
Best Regards,
Iva
Ok, i do migrate due to the migration guide, but i found that the K60D10 files, device specific files and platform files, are already there. So this part is finished fast.
Now i want to check the options at "Build the Platform Library" (page 12), but i can't find the displayed menues. Under project properties there is no "Category" and e. g. no "Assembler". I searched both strings via the "Quick Access" box and the properties search box but got only empty results.
Where can i find the options?
I followed the instructions in the migration guide and found out that for MK60DN256ZVLL10 i have to choose MK60DN256VLL10 because they differ only in the DIE mask version.
But for all projects with this processor there is no support for PE and KDS, even in the example projects in the KSDK 1.2! So there is something still missing which is not mentioned in the guide.
Therefore i tried the other way, creating a project with the board twrk60d100 and switching the processor to type MK60DN256VLL10. This works; i can compile and debug with the Segger USB adapter and have the project with KDS and PE!
Hello Rolf,
I´m very sorry for my late response, but I see yourpost and the answer (with mask revision) from my colleague.
Please, is it now your issue solved or still occurs?
Please, let me know.
Thank you.
Best Regards,
Iva
Yes, the mask revision problem is solved, thanks.
The SDK supported devices are listed in
C:\Freescale\KSDK_1.2.0\ksdk_manifest.xml
And there I see that the variant without the 'Z' is supported by the SDK, but not the one with the 'Z'
Erich