KSKD 1.3 / TWR-K65 / Ethernet Serial Demo
Dear KsDK 1.3 support team,
I am having a bit of problem recompiling the Ethernet to Serial DEmo program for KSKD1.3 / TWR-K65.
The demo prgram is under this folder:
C:\Freescale\KSDK_1.3.0\middleware\tcpip\rtcs\examples\eth_to_serial\build\kds\eth_to_serial_twrk65f180m
As you can see, from my attached screen capture, I have recompiled the lib, platform, rtsc projects.
There is fatal error "There is no such file or directory for Psptypes.h"
include "psptypes.h"
I located where that file an and added to the link resources path for it but it still won't compiled.
Please advise!
Thx,
hy
Hello Mai,
When you want run one MQX demo , and you do not clearly which lib need to be build ,
i recommend you import the project use "MQX->Import Working Sets":
then "build all"
You can see there is no error :
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------