Hi Peter,
I have ported V9.0.0 for the SDK and shared it on GitHub (FRDM-K22F project, but it applies to any Cortex-M0+ or M4(F)) here:
Additionally, I have posted details about it here:
https://mcuoneclipse.com/2016/05/29/freertos-v9-0-0-with-static-memory-allocation/
You simply can drop-in that port (just make sure you are using that new FreeRTOSconfig.h, example in mcuoneclipse/Examples/KDS/FRDM-K22F/FRDM-K22F_USB_Mouse_Kybd_SDK_v2.0/source at master · ErichStyger...
If you are using Processor Expert, you can get a new FreeRTOS from SourceForge, see https://mcuoneclipse.com/2016/05/29/mcuoneclipse-components-29-may-2016-release/. And you can use these components with the Kinetis SDK V2.0 with some limitations as well, see https://mcuoneclipse.com/2016/05/20/tutorial-freertos-with-nxp-kinetis-sdk-v2-0-and-processor-expert...
All above is for the Kinetis SDK V2.0, I have not ported it for the SDK v1.x (where I think it does not make much sense).
I hope this helps,
Erich
Hi Peter,
I have ported V9.0.0 for the SDK and shared it on GitHub (FRDM-K22F project, but it applies to any Cortex-M0+ or M4(F)) here:
Additionally, I have posted details about it here:
https://mcuoneclipse.com/2016/05/29/freertos-v9-0-0-with-static-memory-allocation/
You simply can drop-in that port (just make sure you are using that new FreeRTOSconfig.h, example in mcuoneclipse/Examples/KDS/FRDM-K22F/FRDM-K22F_USB_Mouse_Kybd_SDK_v2.0/source at master · ErichStyger...
If you are using Processor Expert, you can get a new FreeRTOS from SourceForge, see https://mcuoneclipse.com/2016/05/29/mcuoneclipse-components-29-may-2016-release/. And you can use these components with the Kinetis SDK V2.0 with some limitations as well, see https://mcuoneclipse.com/2016/05/20/tutorial-freertos-with-nxp-kinetis-sdk-v2-0-and-processor-expert...
All above is for the Kinetis SDK V2.0, I have not ported it for the SDK v1.x (where I think it does not make much sense).
I hope this helps,
Erich
Hi Erich,
That's great, I'm using SDK V2.0 also.
Much thanks!,
Peter
Hi Peter.
Yes, we have. But at the moment the specific release was not determined.
I will keep you informed.
Best Regards,
Iva