下载程序时出现Device is permanently secure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

下载程序时出现Device is permanently secure

857 Views
yanandren
Contributor II

HI,ALL

 

我在使用keil给我的MKL27Z64VLH4下载程序的时候出现了如下的提示,请问有什么办法可以解除板子的secure.

 

 

谢谢。

 


152779_152779.pngQQ图片20160603124736.png

 

 

152885_152885.pngQQ图片20160603124750.png

Labels (1)
0 Kudos
Reply
2 Replies

739 Views
ivadorazinova
NXP Employee
NXP Employee

Hi YAN.

Thank you for your feedback.

Just click on yes, it should works without problems now.

QQ图片20160603124736.png

Please, let me know if it works you.

Best Regards,

Iva

0 Kudos
Reply

739 Views
yanandren
Contributor II

Hi Iva,

Thanks for the answer.

But the 'Comfirm' dialog showed up twice and then jump to the 'PEMICRO connection manage' dialog.

Only clicked YES can't solve my issue.

Is there any possibility that the Board had been locked ?

BR

Bernerd

0 Kudos
Reply