请问一下,
我在配置KL27ZM64的GPIO口输入或者输出的时候有一个上拉,配置完以后就是默认高电平,请问如何可以不用这个上拉。
承蒙关照。
Hi Bernerd,
请问使用了哪个版本的ksdk?可以贴一段初始化代码上来看看吗?谢谢!
Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
SDK版本:SDK_2.0_FRDM-KL27Z
#define IO_GPIO GPIOB //定义SDA的GPIO
#define IO_PIN 0
#define IO_OUT IO_GPIO->PDDR |= (1U << IO_PIN); //配置输出
#define IO_IN IO_GPIO->PDDR &= ~(1U << IO_PIN); //配置输入
static inline void Slave_Send_Byte(uint8_t snd)
{
uint8_t loop=0;
IO_OUT();
//此处是函数体,就是给IO发送一些bit,发送完以后配置成输入模式
IO_IN();
}