I am designing a brushless DC motor control electronics assembly, and I am conducting bench testing with a hardware setup consisting of a FRDM-MC LVMTR, a FRDM-KV31F, a FRDM-GD3000EVB, and a FRDM-PWRSTG1EVB. I'd like to use MCUXpresso for the IDE and find a project to instantiate on the hardware and evaluate the motor performance, but I have not met with success.
Right now I'm trying to use I'm using the project frdmkv31f_mc_bldc, but all I get is a blinking red D4 LED, and no motor movement.
I'm the electronics hardware engineer on the project (very little software experience), and I only need to spin the motor (under any type of control), verify that the hardware and IDE toolchain will meet our needs, and then I can pass it all along to our software engineers.
Their IDE of choice is MCUXpresso.
Can anyone provide guidance? Thanks!