Hi all,
I am trying to secure kinetis k10 microcontroller. Normally my project works without any problem. If I enable the security option from processor expert, my code does not work. The only thing that I do is enableing the security checkbox below. Probably my code does not start. Any suggestion please...
Okan,
已解决! 转到解答。
Hello Okan,
Are you trying to program or to debug it?
If you just program the board (You can try with Flash file to target in CodeWarrior, the blue thunder icon) it should work.
Regards,
Santiago
Hi Erich,
I use PE Micro multilink. You can find the programmer logs below. I realized that at the bottom of log it is written that "Device is secured. Erasing ...". It says "Erasing" at the end, is it normal.
Starting 3rd party flash programming...
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_OK
INF: Copyright 2012 P&E Microcomputer Systems,Inc.
INF: Command Line :"C:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0
INF: CMD>RE
INF: Initializing.
INF: Target has been RESET and is active.
INF: CMD>CM C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\arm\gdi\P&E\k10dx128m7_pflash_dflash_eeprom_pipeline.arp
INF: Initializing.
INF: Initialized.
INF: ;version 1.04, 02/04/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_128k_dx_pflash_dflash_eeprom_p1_pipeline]
INF: ;device freescale, k10dx128m7, desc=pflash_dflash_eeprom_pipeline
INF: ;begin_cs device=$00000000, length=$14000800, ram=$20000000
INF: Loading programming algorithm ...
INF: Done.
INF: CMD>PA 3601
INF: Started.
INF: Done.
INF: CMD>EM
INF: Erasing.
INF: Module has been erased.
INF: Initializing.
INF: Initialized.
INF: ;version 1.04, 02/04/2014, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_128k_dx_pflash_dflash_eeprom_p1_pipeline]
INF: ;device freescale, k10dx128m7, desc=pflash_dflash_eeprom_pipeline
INF: ;begin_cs device=$00000000, length=$14000800, ram=$20000000
INF: Loading programming algorithm ...
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_PRESERVE_PARTITIONING, Value : 0, R) => DI_ERR_NONFATAL
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_PARTITIONING, Value : 1, R) => DI_OK
INF: Done.
INF: CMD>PM
INF: Programming.
INF: Processing Object File Data ...
INF: .
INF: Programmed.
INF: CMD>VC
INF: Verifying object file CRC-16 to device ranges ...
INF: block 00000000-000001BB ...
INF: Ok.
INF: block 00000400-0000D54B ...
INF: Ok.
INF: Checksum Verification Successful. (Cumulative CRC-16=$449C)
INF: CMD>RE
INF: Initializing.
INF: Device is Secure.
INF: Device is secured. Erasing ...
INF: Target has been RESET and is active.
Hi Okan,
I've found an interesting post on community which can may be help you.
This post refers to 2 ANs:
How (not) to Secure my Microcontroller | MCU on Eclipse
Device is secure? | MCU on Eclipse
Hope this will help.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Pascal,
Thank you for your reply. Actually I dont have problem with programming my board. If I program my board with unsecure device settings, I have no problem and my board works well. If I choose to secure mcu from processor expert and program my device, my board does not work. I made a simple LED blinking project to test it. You can see the source code at previous image. I tested at different boards, same result. Thank you again.
Okan,
Hello Okan,
Are you trying to program or to debug it?
If you just program the board (You can try with Flash file to target in CodeWarrior, the blue thunder icon) it should work.
Regards,
Santiago