is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

is there any difference between 'S32 Design Studio IDE' and 'CW V10.6'?

跳至解决方案
1,281 次查看
taofu
Contributor II

if supported devices quantity is not incorporate, is there any difference between these two IDE?

标签 (1)
0 项奖励
1 解答
833 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
2 回复数
834 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello tao

S32DS is:

−Low-cost / No-cost Software Development Tool Strategy

−Low-Cost to develop and maintain

•No-Cost to our customers

•GCC Base Compiler Performance

•Intended to complement and enable Third-Party Partner Tools (Compilers & Debuggers)

•Support for Premium compilers addressing Automotive

Safety Requirements (GHS, Cosmic,...)

•Integration of Freescale software in easy to use

environment for application development (AMMCLIB, MCAT... )

IS NOT

•KDS Equivalent

•AUTOSAR software

•CodeWarrior Replacement

•Premium Tool Replacement (w/ Advanced Debugging,

Best in class code performance, etc...)

S32DS is Basic Tool Frame Work which includes:

• GNU C/C++ Compiler (GCC from ARM Cortex-M and A cores,

GCC for Power Architecture, Standard Solid Compilers)

•Basic Eclipse Backplane

•GNU GDB Debugger:  Basic Debugger interface to low cost JTAG debugger

(Pemicro, Segger, and OpenOCD)

CodeWarrior supports multiple architecture (S08,RS08,S12,S12X,S12Z,DSC,Coldfire, PowerPC and Kinetis) . CodeWarrior comes with its own compiler, proprietary ANSI and runtime library, and is using a proprietary debugger engine. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
833 次查看
taofu
Contributor II

thank you very much, it is very helpful for me.

0 项奖励