PORT_SetPinInterruptConfig(PORTA, 4U, kPORT_InterruptLogicZero);void SysTick_Handler(void)
{GPIO_PortToggle(BOARD_LED_GPIO, 1u << BOARD_LED_GPIO_PIN);}void PORTA_IRQHandler(void) {
GPIO_ClearPinsInterruptFlags(GPIOA, 1U << 4);
}
Hi Luca
The KV58 is an advanced Cortex-M7 part which is not used by many people. It is not included in the Open Source version and only a basic (untested) port is presently available in the developer's version(!)
I don't have a TWR-KV58V220M and so have only simulated it (see below):
Although many modules are compatible with other parts, the KV58 has various new ones that are unique to it, which i haven't integrated. Since the module addresses do get moved around between different devices I expect that the basic port (which will do UARTs, Ethernet, port interrupts, low power modes, PITs, LPTMR, FlexTimers ad maybe a few more such generic modules) will probably fail on first attempts on the HW since something hasn't been spotted yet that needs a special setting. Sometimes it does work on first attempt but the KV58 is rather complex so the chances are lower. Fixing such things is easy though, but needs the HW tests to show it.
I'll give you access to the developer's version (which will simulate and run on around 80 development boards) so you can have a look at it and if you feel up to it you could see whether you can get the KV58 tweaked to work. I'll send you my email too so you can inform me of any issues so that I can point you in the correct direction at the beginning.
Regards
Mark
Hi Luca
When you configure the interrupt you can give it a priority - if the Systck's interrupt has a "lower" priority value than the GPIO port interrupt it will interrupt the other.
Regards
Mark
Hi Luca
I use the uTasker project where the priorities are set with (for example):
#define SYSTICK_PRIORITY 2
#define PRIORITY_PORT_A_INT 6
#define PRIORITY_PORT_B_INT 5
#define PRIORITY_PORT_C_INT 7
#define PRIORITY_PORT_D_INT 9
#define PRIORITY_PORT_E_INT 9
If you are using another framework you will need to read its documentation or study its code, or wait for a response from someone managing its support.
Regards
Mark
Luca
In the uTasker project I can do this:
1) Configure two port outputs for test purposes:
extern void fnUserHWInit(void)
{
_CONFIG_DRIVE_PORT_OUTPUT_VALUE(C, (PORTC_BIT3 | PORTC_BIT4), (PORTC_BIT3 | PORTC_BIT4), (PORT_SRE_SLOW | PORT_DSE_HIGH));
}
2) Configure a 100us SYSTICK with high priority:
#define _TICK_RESOLUTION TICK_UNIT_US(100)
#define SYSTICK_PRIORITY 1
3) Configure an input with level sensitive interrupt at lower priority
#define PRIORITY_PORT_A_INT 6
static void fnInitIRQ(void)
{
INTERRUPT_SETUP interrupt_setup; // interrupt configuration parameters
interrupt_setup.int_type = PORT_INTERRUPT; // identifier to configure port interrupt
interrupt_setup.int_handler = test_irq; // handling function
interrupt_setup.int_priority = PRIORITY_PORT_A_INT; // interrupt priority level
interrupt_setup.int_port = PORTA; // the port that the interrupt input is on
interrupt_setup.int_port_bits = PORTA_BIT10; // the IRQ input connecte
interrupt_setup.int_port_sense = (IRQ_LOW_LEVEL | PULLUP_ON);// interrupt is to be low level sensitive
fnConfigureInterrupt((void *)&interrupt_setup); // configure interrupt
}
4) In the SYSTICK interrupt handler I toggle one port each times it enters and in the IRQ handler I toggle the other port on each entry:
static __interrupt void _RealTimeInterrupt(void)
{
_TOGGLE_PORT(C, PORTC_BIT3);
..
}
static void __callback_interrupt test_irq(void)
{
_TOGGLE_PORT(C, PORTC_BIT4);
}
When I run this and press the input with level sensitive input this is the output that is recorded:
As can be seen, the 100us SYSTICK is still executed even when there is a continuous level sensitive interrupt on the input due to the fact that it has a higher interrupt priority and takes priority when both are pending and it also pre-empts the port interrupt handler.
If I then do
#define SYSTICK_PRIORITY 7
the result is
where it is seen that the SYSTICK interrupt is not called any more due to the fact that the port interrupt is always pending and has priority.
Regards
Mark