have the K20 and K24 families the same USB cell? is there the same hw architecture?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

have the K20 and K24 families the same USB cell? is there the same hw architecture?

515件の閲覧回数
manricoprevital
Contributor I

I have to use a particular (not NXP) USB stack.

I have used this stack for kinesis K20 familiy.

Are the same USB HW cell in the K20 and K24 family?

0 件の賞賛
返信
1 返信

455件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

No, K24_120: USB 2.0 On-The-Go (full-speed) with USB transceiver.

K20_120: USB 2.0 On-The-Go (full and high speed).Current/time for portable USB devices enabling longer battery life. 

So they are different.

0 件の賞賛
返信