eGUI using K70's LCDC and any TFT LCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eGUI using K70's LCDC and any TFT LCD

3,028 Views
ángelbarragán
Contributor I

Hi,

     I'm fairly new to the programming of Freescale's microcontrollers and for a project that I will soon start working on, the intention is to implement the K70's LCDC with any TFT LCD. I see that there is a software library called eGUI, however, all the eGUI implementation examples that I've seen on the web only include the K70 twr-kit and the twr-lcd or twr-lcd-RGB module. My question is: Is it possible to implement eGUI with any K70's LCDC and any TFT LCD without using twr kits? Thanks in advance.

Labels (1)
2 Replies

2,808 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Of course, you can. You can reuse everything except the particular parameters of your TFT panel and resize the frame buffer to the panel resolution. See attached file.

Luis

2,808 Views
ángelbarragán
Contributor I

Hello Luis,

     First of all I would like to thank you for your fast response. It really help me out a lot. One last question, if the K70 already has an LCDC, then I must purchase an TFT LCD without a controller like the SSD1963, right? Thanks for taking your time in responding my questions.

Ángel

0 Kudos
Reply