Why the I2S MCLK output frequency of KL26 is not correct?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the I2S MCLK output frequency of KL26 is not correct?

1,497件の閲覧回数
2743294708
Contributor I

Dear,

In my design, the MCLK is mapped to PTC4. The epected frequency of MCLK is 12.288MHz, divided from PLL_CLK 48MHz.

But when configured, the output frequency of MCLK on PTC4 pin, is always 48MHz, although the MDR regisiter is set to deifferent values, it seems that the MDR value doesn't work.

The clock configure code is as follow. Please help check why the MCLK is not 12.288MHz.

    CLOCK_EnableClock( kCLOCK_Sai0 );

    //master clock source: PLL_CLK, MCR[MICS] = 11b
    I2S0->MCR |= I2S_MCR_MICS(3);

    //Enable MCLK output, MCR[MOE] = 1b
    I2S0->MCR |= I2S_MCR_MOE(1);
    
    //Set the FRACT and DIVIDE. MCLK = master clock/(FRACT+1)/(DIVIDE+1), FRACT = 255, DIVIDE = 999
    I2S0->MCR &= ~I2S_MCR_DUF_MASK;
    I2S0->MDR =( I2S_MDR_DIVIDE(1000 - 1)  |  I2S_MDR_FRACT(256 - 1) );

    while( I2S0->MCR & I2S_MCR_DUF_MASK ){                // check MCR[DUF]
    }
   
    //TCR2[MSEL](27-26) = 01b, TCR2[BCD](24) = 1b, DIV(7-0) = 4/2-1 = 1
    I2S0->TCR2 |= (0x00000001<<26) | (0x00000001<<24) | (0x00000001);
    
    //Rx clock set, internally generated, Rx BCLK = MCLK/4, 12.288M = 3.072*4 = 48K*32*2
    I2S0->RCR2 |= (0x00000001<<26) | (0x00000001<<24) | (0x00000001);

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,246件の閲覧回数
2743294708
Contributor I

I think I have found the answer in another question: Does the KL26 have a fractional clock divider for use with I2S? 

The same description is also found in the document "KL26P121M48SF4RM", page 114, "The module's MCLK Divide Register (MDR) is not used to control MCLK generation".

Please confirm again, does that mean the KL26 doesn't support fractional clock divider?

0 件の賞賛
返信

1,246件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Correct. The KL26 doesn't support fractional clock divider as you mentioned.

1,246件の閲覧回数
2743294708
Contributor I

OK,it's clear.

Thanks for your reply.

0 件の賞賛
返信