Where I can find DAPLink for MIMXRT1064-EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where I can find DAPLink for MIMXRT1064-EVK?

Jump to solution
2,016 Views
tonimerino
Contributor II

Where I can find DAPLink for MIMXRT1064-EVK?

Tags (1)
1 Solution
1,727 Views
BlackNight
NXP Employee
NXP Employee

Hi Toni,

seems to be an issue with the web page. I have attached the two files for you....

Erich

View solution in original post

9 Replies
1,727 Views
BlackNight
NXP Employee
NXP Employee

Not sure what you exactly mean, but the DAPLink is embedded on the i.MX RT1064-EVK, see First Steps with the NXP i.MX RT1064-EVK Board | MCU on Eclipse . You can use it with the the DAPLink firmware or (what I prefer) as a LPC-Link2 (see as well above article).

I hope this helps,

Erich

0 Kudos
1,727 Views
tonimerino
Contributor II

Hi Erich,

I am looking for DAPLink firmware for MIMXRT1064EVK

After using firmware for RT1060, my board appears to upload programs but not running the program uploaded.

I have search this page:

OpenSDA Serial and Debug Adapter|NXP 

but RT1064 not appears listed. Is not available?

Regards.

0 Kudos
1,727 Views
BlackNight
NXP Employee
NXP Employee

Hi Toni,

to my understanding it should be uploaded there probably in a few days.

0 Kudos
1,727 Views
tonimerino
Contributor II

Thanks Erich, time to wait...

0 Kudos
1,727 Views
BlackNight
NXP Employee
NXP Employee

Hi Toni,

checked again today, and the files are now on the server.

Erich

0 Kudos
1,727 Views
tonimerino
Contributor II

Thx Erich

First I get a 404 error on links, now I get 0 Bytes files... :smileysad:

Regards

0 Kudos
1,728 Views
BlackNight
NXP Employee
NXP Employee

Hi Toni,

seems to be an issue with the web page. I have attached the two files for you....

Erich

1,727 Views
tonimerino
Contributor II

Hi Erich,

A million thanks.  :smileyhappy:

Regards

0 Kudos
1,727 Views
BlackNight
NXP Employee
NXP Employee

Hi Toni,

I see that the board is now listed on

OpenSDA Serial and Debug Adapter|NXP

(but the links to the files are not there yet).

0 Kudos